Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.tooldesigner |
Provides classes and interfaces for ToolDesigner.
|
Modifier and Type | Method and Description |
---|---|
SubsetBuilder |
CollaborativeDesignCollection.currentSubsetBuilder()
Returns the
SubsetBuilder used to edit the current subset in the
subset task environment
License requirements: assemblies ("ASSEMBLIES MODULE") Created in NX8.5.0 |
Modifier and Type | Method and Description |
---|---|
SubsetBuilder |
SubsetCollection.createSubsetBuilder(Subset subset)
Creates an
SubsetBuilder
License requirements: nx_4gd_integration ("4th Generation Design") Created in NX8.5.0 |
SubsetBuilder |
MechanicalRoutingSubsetBuilder.getSearchSubsetBuilder()
The subset builder which is used for searching runs, the user will have to use
FindInCollaborativeDesign to search for runs
using object type RunElement. |
SubsetBuilder |
MechanicalRoutingSubsetBuilder.updateSubsetUsingConfigurationContext(SubsetBuilder inputSubsetBuilder)
The routing subsets will be updated (e.g. revision rule, effectivity) using the information available on the
ConfigurationContext if the input is NULL.
|
Modifier and Type | Method and Description |
---|---|
MechanicalRoutingSubsetBuilder |
SubsetCollection.createMechanicalRoutingSubsetBuilder(SubsetBuilder subsetBuilderTag)
Creates an
MechanicalRoutingSubsetBuilder . |
MechanicalRoutingSubsetBuilder |
SubsetCollection.createMechanicalRoutingSubsetBuilderForSurroundingEdit(SubsetBuilder subsetBuilderTag)
Creates an
MechanicalRoutingSubsetBuilder . |
void |
MechanicalRoutingSubsetBuilder.setSearchSubsetBuilder(SubsetBuilder subsetBuilder)
Sets the subset builder which needs to be set by user to search runs, the user will have to use
FindInCollaborativeDesign to search for runs
using object type RunElement. |
SubsetBuilder |
MechanicalRoutingSubsetBuilder.updateSubsetUsingConfigurationContext(SubsetBuilder inputSubsetBuilder)
The routing subsets will be updated (e.g. revision rule, effectivity) using the information available on the
ConfigurationContext if the input is NULL.
|
Modifier and Type | Method and Description |
---|---|
SubsetBuilder |
SelectWeldsBuilder.getCurrentSubsetBuilder()
GetCurrentSubsetBuilder
License requirements: fp_fixture_planner ("FULL FIXTURE PLANNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.