Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static RelinkerBuilder.LinkOption |
RelinkerBuilder.LinkOption.BOTH
Indicate relink option is both interpart expression and wave link
|
static RelinkerBuilder.LinkOption |
RelinkerBuilder.LinkOption.INTERPART_EXPRESSION
Indicate relink option is interpart expression only
|
static RelinkerBuilder.LinkOption |
RelinkerBuilder.LinkOption.WAVE_GEOMETRY
Indicate relink option is wave geometry only
|
Modifier and Type | Method and Description |
---|---|
RelinkerBuilder.LinkOption |
RelinkerBuilder.relinkOption()
Returns the link option.
|
static RelinkerBuilder.LinkOption |
RelinkerBuilder.LinkOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RelinkerBuilder.LinkOption |
RelinkerBuilder.LinkOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RelinkerBuilder.LinkOption[] |
RelinkerBuilder.LinkOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RelinkerBuilder.setRelinkOption(RelinkerBuilder.LinkOption linkOption)
License requirements: wave ("WAVE FUNCTIONALITY") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.