Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Method and Description |
---|---|
Explosion |
Traceline.askExplosion()
Returns the explosion that the traceline has been created in
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Modifier and Type | Method and Description |
---|---|
AutomaticTraceline |
TracelineCollection.createAutomaticTraceline(Explosion explosion,
Point startPoint,
Direction startDirection,
Point endPoint,
Direction endDirection,
Matrix3x3 orientation,
AutomaticTraceline.ModeOption mode,
int solution,
double startOffset,
double endOffset,
int[] segmentIndices,
double[] segmentLengths)
Create an automatic traceline
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Xform |
XformCollection.createXform(Explosion explosion,
Component sourceComponent,
Component destComponent,
SmartObject.UpdateOption updateOption)
Creates an Xform based on the delta difference between the source and
destination components in the explosion.
|
Xform |
XformCollection.createXform(NXObject object,
Explosion explosion,
SmartObject.UpdateOption updateOption)
Creates an Xform based on an object and an explosion.
|
Modifier and Type | Method and Description |
---|---|
Explosion |
ExplosionCollection.create(String explosionName)
Creates an explosion based upon the default arrangement in the given OCC part.
|
Explosion |
ExplosionCollection.findObject(String name)
Finds the
Explosion with the given identifier as recorded in a journal. |
Explosion |
ExplodedComponent.getExplosion()
Gets the
Explosion associated with the exploded component. |
Modifier and Type | Method and Description |
---|---|
void |
Explosion.copy(Explosion destinationExplosion)
Copies the component transformations in the source explosion onto the destination explosion.
|
Modifier and Type | Method and Description |
---|---|
Explosion |
PostProcess.explodeMechanism(String explosionName)
Explode mechanism
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.