Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ComponentAssembly.SubstitutionMode |
ComponentAssembly.SubstitutionMode.ALL
An associative substitution is performed on all components that
represent the same prototype part.
|
static ComponentAssembly.SubstitutionMode |
ComponentAssembly.SubstitutionMode.NON_ASSOCIATIVE
The old component is deleted, and the new one is added
|
static ComponentAssembly.SubstitutionMode |
ComponentAssembly.SubstitutionMode.SINGLE_COMPONENT
An associative substitution is performed.
|
Modifier and Type | Method and Description |
---|---|
static ComponentAssembly.SubstitutionMode |
ComponentAssembly.SubstitutionMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentAssembly.SubstitutionMode |
ComponentAssembly.SubstitutionMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentAssembly.SubstitutionMode[] |
ComponentAssembly.SubstitutionMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Component |
ComponentAssembly.substituteComponent(Component component,
BasePart part,
String newName,
String referenceSet,
int layer,
ComponentAssembly.SubstitutionMode mode)
Substitutes an old component with a new component.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.