Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static Component.RepresentationMode |
Component.RepresentationMode.EXACT
The component's solid bodies are displayed with the exact data
|
static Component.RepresentationMode |
Component.RepresentationMode.LIGHTWEIGHT
The component's solid bodies are all displayed using the lightweight representation
|
static Component.RepresentationMode |
Component.RepresentationMode.NONE
There are no bodies to display for the current component
|
static Component.RepresentationMode |
Component.RepresentationMode.PARTIAL
The component's solid bodies are displayed with some being exact and some being shown lightweight
|
Modifier and Type | Method and Description |
---|---|
Component.RepresentationMode |
Component.getComponentRepresentationMode()
Returns the representation mode for the component's bodies.
|
static Component.RepresentationMode |
Component.RepresentationMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Component.RepresentationMode |
Component.RepresentationMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Component.RepresentationMode[] |
Component.RepresentationMode.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.