Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ClearanceAnalysisBuilder.ClearanceBetweenEntity |
ClearanceAnalysisBuilder.ClearanceBetweenEntity.BODIES |
static ClearanceAnalysisBuilder.ClearanceBetweenEntity |
ClearanceAnalysisBuilder.ClearanceBetweenEntity.COMPONENTS |
Modifier and Type | Method and Description |
---|---|
ClearanceAnalysisBuilder.ClearanceBetweenEntity |
ClearanceAnalysisBuilder.clearanceBetween()
Returns the setting to determine whether components or bodies should be used.
|
static ClearanceAnalysisBuilder.ClearanceBetweenEntity |
ClearanceAnalysisBuilder.ClearanceBetweenEntity.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceAnalysisBuilder.ClearanceBetweenEntity |
ClearanceAnalysisBuilder.ClearanceBetweenEntity.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceAnalysisBuilder.ClearanceBetweenEntity[] |
ClearanceAnalysisBuilder.ClearanceBetweenEntity.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ClearanceAnalysisBuilder.setClearanceBetween(ClearanceAnalysisBuilder.ClearanceBetweenEntity clearanceBetweenEntity)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.