public static class ComponentAssembly.CheckinCheckoutOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOTH
Checks in or Checks out the design element and its referenced source item
|
static int |
_DEFAULT
Check In or Check Out option is determined by the system using whatever option is appropriate for the selected object type.
|
static int |
_DESIGN_ELEMENT
Checks in or Checks out the design element
|
static int |
_SOURCE_ITEM
Checks in or Checks out the source item that is referenced by a reuse design element or subordinate design element
|
static ComponentAssembly.CheckinCheckoutOption |
BOTH
Checks in or Checks out the design element and its referenced source item
|
static ComponentAssembly.CheckinCheckoutOption |
DEFAULT
Check In or Check Out option is determined by the system using whatever option is appropriate for the selected object type.
|
static ComponentAssembly.CheckinCheckoutOption |
DESIGN_ELEMENT
Checks in or Checks out the design element
|
static ComponentAssembly.CheckinCheckoutOption |
SOURCE_ITEM
Checks in or Checks out the source item that is referenced by a reuse design element or subordinate design element
|
Modifier and Type | Method and Description |
---|---|
static ComponentAssembly.CheckinCheckoutOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentAssembly.CheckinCheckoutOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentAssembly.CheckinCheckoutOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final ComponentAssembly.CheckinCheckoutOption DESIGN_ELEMENT
public static final ComponentAssembly.CheckinCheckoutOption SOURCE_ITEM
public static final ComponentAssembly.CheckinCheckoutOption BOTH
public static final ComponentAssembly.CheckinCheckoutOption DEFAULT
public static final int _DESIGN_ELEMENT
public static final int _SOURCE_ITEM
public static final int _BOTH
public static final int _DEFAULT
public static ComponentAssembly.CheckinCheckoutOption valueOf(int value)
public static ComponentAssembly.CheckinCheckoutOption valueOf(String name)
public static ComponentAssembly.CheckinCheckoutOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.