Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static ZeroToleranceDisplayStyle |
ZeroToleranceDisplayStyle.AS_ZERO
Always display zero tolerance as 0
|
static ZeroToleranceDisplayStyle |
ZeroToleranceDisplayStyle.BASED_ON_UNITS
Zero tolerance display is tied to display units
|
static ZeroToleranceDisplayStyle |
ZeroToleranceDisplayStyle.OMITTED
Omit the display of zero tolerance and maintain position of remaining tolerance
|
static ZeroToleranceDisplayStyle |
ZeroToleranceDisplayStyle.OMITTED_AND_INLINED
Omit the display of zero tolerance and inline the remaining tolerance
|
Modifier and Type | Method and Description |
---|---|
ZeroToleranceDisplayStyle |
DimensionStyleBuilder.dimZeroToleranceDisplayStyle()
Returns the dimension zero tolerance display style
License requirements: None. |
static ZeroToleranceDisplayStyle |
ZeroToleranceDisplayStyle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ZeroToleranceDisplayStyle |
ZeroToleranceDisplayStyle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ZeroToleranceDisplayStyle[] |
ZeroToleranceDisplayStyle.values()
Returns an array that contains the values for this enum.
|
ZeroToleranceDisplayStyle |
LinearTolerance.zeroToleranceDisplayStyle()
Returns the zero tolerance display style
License requirements: None. |
ZeroToleranceDisplayStyle |
DimensionPreferences.zeroToleranceDisplayStyle()
Deprecated.
Deprecated in NX7.5.0. Use
LinearTolerance.zeroToleranceDisplayStyle() for linear dimensions and AngularTolerance.zeroToleranceDisplayStyle() for angular dimensions instead.
|
ZeroToleranceDisplayStyle |
AngularTolerance.zeroToleranceDisplayStyle()
Returns the zero tolerance display style
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DimensionStyleBuilder.setDimZeroToleranceDisplayStyle(ZeroToleranceDisplayStyle dimZeroToleranceDisplayStyle)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
LinearTolerance.setZeroToleranceDisplayStyle(ZeroToleranceDisplayStyle zeroDisplayStyle)
License requirements: None. |
void |
DimensionPreferences.setZeroToleranceDisplayStyle(ZeroToleranceDisplayStyle zeroDisplayStyle)
Deprecated.
Deprecated in NX7.5.0. Use
LinearTolerance.setZeroToleranceDisplayStyle(nxopen.annotations.ZeroToleranceDisplayStyle) for linear dimensions and AngularTolerance.setZeroToleranceDisplayStyle(nxopen.annotations.ZeroToleranceDisplayStyle) for angular dimensions instead.
|
void |
AngularTolerance.setZeroToleranceDisplayStyle(ZeroToleranceDisplayStyle zeroDisplayStyle)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.