Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static WeldStandard |
WeldStandard.ANSI
ANSI standard
|
static WeldStandard |
WeldStandard.DIN
DIN standard
|
static WeldStandard |
WeldStandard.ESKD
ESKD standard
|
static WeldStandard |
WeldStandard.GB
GB standard
|
static WeldStandard |
WeldStandard.ISO
ISO standard
|
static WeldStandard |
WeldStandard.JIS
JIS standard
|
static WeldStandard |
WeldStandard.LAST
Last enum value.
|
Modifier and Type | Method and Description |
---|---|
static WeldStandard |
WeldStandard.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldStandard |
WeldStandard.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldStandard[] |
WeldStandard.values()
Returns an array that contains the values for this enum.
|
WeldStandard |
LineWeldData.weldStandard()
Returns the standard
License requirements: None. |
WeldStandard |
AnnotationManager.weldStandard()
Returns the weld standard for the part file.
|
WeldStandard |
SymbolStyleBuilder.weldSymbolStandard()
Returns the weld symbol standard
License requirements: None. |
WeldStandard |
SymbolPreferences.weldSymbolStandard()
Returns the weld symbol standard
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LineWeldData.setWeldStandard(WeldStandard standard)
License requirements: None. |
void |
AnnotationManager.setWeldStandard(WeldStandard standard)
Sets the weld standard for the part file.
|
void |
SymbolStyleBuilder.setWeldSymbolStandard(WeldStandard standard)
Sets the weld symbol standard
License requirements: None. |
void |
SymbolPreferences.setWeldSymbolStandard(WeldStandard standard)
Sets the weld symbol standard
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.