Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LineWeld
Represents a line weld
To create or edit an instance of this class, use LineWeldBuilder Created in NX4.0.0 |
interface |
PmiLineWeld
Represents a PMI line weld
To create or edit an instance of this class, use PmiLineWeldBuilder Created in NX4.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
LineWeldBuilder.inheritProperties(Weld annotation)
This inherits the properties from the existing weld symbol
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.