Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
TitleBlockCellBuilder |
TitleBlockCollection.createCellBuilder(DisplayableObject object,
boolean isLocked,
int contentType,
String value,
String label,
boolean canLockStatusChange)
Creates a cell builder
License requirements: None. |
TitleBlockCellBuilder |
TitleBlockCellBuilderList.findItem(int index)
Returns the object at the input index.
|
TitleBlockCellBuilder[] |
TitleBlockCellBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TitleBlockCellBuilderList.append(TitleBlockCellBuilder object)
Appends an object to the list
License requirements: None. |
void |
TitleBlockCellBuilderList.append(TitleBlockCellBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TitleBlockCellBuilderList.erase(TitleBlockCellBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
TitleBlockCellBuilderList.erase(TitleBlockCellBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TitleBlockCellBuilderList.findIndex(TitleBlockCellBuilder obj)
Finds the index where the input object appears.
|
void |
TitleBlockCellBuilderList.insert(int location,
TitleBlockCellBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
TitleBlockCellBuilderList.setContents(TitleBlockCellBuilder[] objects)
Sets the contents of the entire list.
|
void |
TitleBlockCellBuilderList.swap(TitleBlockCellBuilder object1,
TitleBlockCellBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.