Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static TextWithSymbolsBuilder.SymbolSizingMethod |
TextWithSymbolsBuilder.SymbolSizingMethod.LENGTH_AND_HEIGHT
Size using length and height
|
static TextWithSymbolsBuilder.SymbolSizingMethod |
TextWithSymbolsBuilder.SymbolSizingMethod.SCALE_AND_ASPECT_RATIO
Size using scale and aspect ratio
|
Modifier and Type | Method and Description |
---|---|
TextWithSymbolsBuilder.SymbolSizingMethod |
TextWithSymbolsBuilder.symbolSizeMethod()
Returns the method in which embedded user-defined symbols are scaled
License requirements: None. |
static TextWithSymbolsBuilder.SymbolSizingMethod |
TextWithSymbolsBuilder.SymbolSizingMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextWithSymbolsBuilder.SymbolSizingMethod |
TextWithSymbolsBuilder.SymbolSizingMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextWithSymbolsBuilder.SymbolSizingMethod[] |
TextWithSymbolsBuilder.SymbolSizingMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TextWithSymbolsBuilder.setSymbolSizeMethod(TextWithSymbolsBuilder.SymbolSizingMethod symbolSizeMethod)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.