Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.ANCHOR_POINT
Anchor Point
|
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.BOTTOM
Bottom
|
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.MIDDLE
Middle
|
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.NONE
None
|
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.TOP
Top
|
Modifier and Type | Method and Description |
---|---|
TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.getSymbolAlignment(String symbolName)
Get the alignement of embedded symbol correspoding to symbol name
License requirements: None. |
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TextWithSymbolsBuilder.SymbolAlignmentType |
TextWithSymbolsBuilder.SymbolAlignmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TextWithSymbolsBuilder.SymbolAlignmentType[] |
TextWithSymbolsBuilder.SymbolAlignmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TextWithSymbolsBuilder.setSymbolAlignment(String symbolName,
TextWithSymbolsBuilder.SymbolAlignmentType symbolAlignment)
Set the alignement on embedded symbol correspoding to symbol name
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.