Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static TableSectionStyleBuilder.LocationOfHeader |
TableSectionStyleBuilder.LocationOfHeader.ABOVE
Above
|
static TableSectionStyleBuilder.LocationOfHeader |
TableSectionStyleBuilder.LocationOfHeader.BELOW
Below
|
static TableSectionStyleBuilder.LocationOfHeader |
TableSectionStyleBuilder.LocationOfHeader.NONE
None
|
Modifier and Type | Method and Description |
---|---|
TableSectionStyleBuilder.LocationOfHeader |
TableSectionStyleBuilder.headerLocation()
Returns the value that represents the location of header on a section
License requirements: None. |
static TableSectionStyleBuilder.LocationOfHeader |
TableSectionStyleBuilder.LocationOfHeader.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TableSectionStyleBuilder.LocationOfHeader |
TableSectionStyleBuilder.LocationOfHeader.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TableSectionStyleBuilder.LocationOfHeader[] |
TableSectionStyleBuilder.LocationOfHeader.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TableSectionStyleBuilder.setHeaderLocation(TableSectionStyleBuilder.LocationOfHeader headerLocation)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.