Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.TimeFormatTypes.HHMM12
12 hh:mm AM/PM
|
static TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.TimeFormatTypes.HHMM24
24 hh:mm
|
static TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.TimeFormatTypes.HHMMSS12
12 hh:mm:ss AM/PM
|
static TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.TimeFormatTypes.HHMMSS24
24 hh:mm:ss
|
Modifier and Type | Method and Description |
---|---|
TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.timeFormatType()
Returns the cell time format.
|
static TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.TimeFormatTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TableCellStyleBuilder.TimeFormatTypes |
TableCellStyleBuilder.TimeFormatTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TableCellStyleBuilder.TimeFormatTypes[] |
TableCellStyleBuilder.TimeFormatTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TableCellStyleBuilder.setTimeFormatType(TableCellStyleBuilder.TimeFormatTypes timeFormat)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.