Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
SymbolCatalogParameterBuilder |
SymbolCatalogParameterBuilderList.findItem(int index)
Returns the object at the input index.
|
SymbolCatalogParameterBuilder[] |
SymbolCatalogParameterBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
SymbolCatalogParameterBuilder |
SymbolCatalogBuilder.newParameter()
Creates a
SymbolCatalogParameterBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
SymbolCatalogParameterBuilderList.append(SymbolCatalogParameterBuilder object)
Appends an object to the list
License requirements: None. |
void |
SymbolCatalogParameterBuilderList.append(SymbolCatalogParameterBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SymbolCatalogParameterBuilderList.erase(SymbolCatalogParameterBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SymbolCatalogParameterBuilderList.erase(SymbolCatalogParameterBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SymbolCatalogParameterBuilderList.findIndex(SymbolCatalogParameterBuilder obj)
Finds the index where the input object appears.
|
void |
SymbolCatalogParameterBuilderList.insert(int location,
SymbolCatalogParameterBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SymbolCatalogParameterBuilderList.setContents(SymbolCatalogParameterBuilder[] objects)
Sets the contents of the entire list.
|
void |
SymbolCatalogParameterBuilderList.swap(SymbolCatalogParameterBuilder object1,
SymbolCatalogParameterBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.