Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static SurfaceFinishStandard |
SurfaceFinishStandard.ANSI
ANSI
|
static SurfaceFinishStandard |
SurfaceFinishStandard.DIN
DIN
|
static SurfaceFinishStandard |
SurfaceFinishStandard.DIN2002
DIN 2002
|
static SurfaceFinishStandard |
SurfaceFinishStandard.ESKD
ESKD
|
static SurfaceFinishStandard |
SurfaceFinishStandard.GB
GB131-93
|
static SurfaceFinishStandard |
SurfaceFinishStandard.ISO
ISO
|
static SurfaceFinishStandard |
SurfaceFinishStandard.ISO2002
ISO 2002
|
static SurfaceFinishStandard |
SurfaceFinishStandard.JIS
JIS
|
Modifier and Type | Method and Description |
---|---|
SurfaceFinishStandard |
SymbolStyleBuilder.draftingSurfaceFinishStandard()
Returns the standard
License requirements: None. |
SurfaceFinishStandard |
SymbolPreferences.draftingSurfaceFinishStandard()
Returns the drafting surface finish standard
License requirements: None. |
static SurfaceFinishStandard |
SurfaceFinishStandard.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceFinishStandard |
SurfaceFinishStandard.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceFinishStandard[] |
SurfaceFinishStandard.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SymbolStyleBuilder.setDraftingSurfaceFinishStandard(SurfaceFinishStandard standard)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
SymbolPreferences.setDraftingSurfaceFinishStandard(SurfaceFinishStandard standard)
Sets the drafting surface finish standard
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.