Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.CREATE_EXPRESSION_FOR_EACH
Creates expressions for controlling the suppression
of each selected PMI object.
|
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.CREATE_SHARED_EXPRESSION
Creates a single expression for controlling
the suppression of the selected PMI objects and
suppresses them.
|
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.MANUAL
Suppress selected PMI objects.
|
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.NONE
Unsuppress selected PMI objects.
|
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.SELECT_EXPRESSION
Allows selection of an expression to control the
suppression of the selected PMI objects.
|
Modifier and Type | Method and Description |
---|---|
SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.suppressionMethod()
Returns the suppression method
License requirements: None. |
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SuppressPMIBuilder.SuppressionMethodType |
SuppressPMIBuilder.SuppressionMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SuppressPMIBuilder.SuppressionMethodType[] |
SuppressPMIBuilder.SuppressionMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SuppressPMIBuilder.setSuppressionMethod(SuppressPMIBuilder.SuppressionMethodType suppressionMethod)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.