Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.LEAST_MATERIAL_CONDITION
least material condition
|
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.MAXIMUM_MATERIAL_CONDITION
maximum material condition
|
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.NONE
none
|
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.REGARDLESSOF_FEATURE_SIZE
regardless of feature size
|
Modifier and Type | Method and Description |
---|---|
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.toleranceMCMType()
Returns the tolerance mcmenum
License requirements: None. |
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions[] |
SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SearchCriteriaFeatureControlFrameBuilder.setToleranceMCMType(SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMOptions toleranceMCMType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.