Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions |
SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions.COMPOSITE_FRAME
composite frame
|
static SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions |
SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions.SINGLE_FRAME
single frame
|
Modifier and Type | Method and Description |
---|---|
SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions |
SearchCriteriaFeatureControlFrameBuilder.frameStyleType()
Returns the frame style enum
License requirements: None. |
static SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions |
SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions |
SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions[] |
SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SearchCriteriaFeatureControlFrameBuilder.setFrameStyleType(SearchCriteriaFeatureControlFrameBuilder.FrameStyleOptions frameStyleType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.