Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static RegionBuilder.CrosshatchPatterns |
RegionBuilder.CrosshatchPatterns.GENERAL_USE
general use
|
static RegionBuilder.CrosshatchPatterns |
RegionBuilder.CrosshatchPatterns.NONE
none
|
Modifier and Type | Method and Description |
---|---|
RegionBuilder.CrosshatchPatterns |
RegionBuilder.crosshatchPattern()
Deprecated.
Deprecated in NX8.5.0. Use
RegionBuilder.crosshatchSettings() instead.
|
static RegionBuilder.CrosshatchPatterns |
RegionBuilder.CrosshatchPatterns.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RegionBuilder.CrosshatchPatterns |
RegionBuilder.CrosshatchPatterns.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RegionBuilder.CrosshatchPatterns[] |
RegionBuilder.CrosshatchPatterns.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RegionBuilder.setCrosshatchPattern(RegionBuilder.CrosshatchPatterns crosshatchPattern)
Deprecated.
Deprecated in NX8.5.0. Use the sublock of
RegionBuilder.crosshatchSettings() called Pattern instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.