Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
HorizontalOrdinateDimension
Represents a horizontal ordinate dimension
To create or edit an instance of this class, use OrdinateDimensionBuilder Created in NX4.0.0 |
interface |
PmiHorizontalOrdinateDimension
Represents a PMI horizontal ordinate dimension
To create or edit an instance of this class, use PmiOrdinateDimensionBuilder Created in NX4.0.0 |
interface |
PmiVerticalOrdinateDimension
Represents a PMI vertical ordinate dimension
To create or edit an instance of this class, use PmiOrdinateDimensionBuilder Created in NX4.0.0 |
interface |
VerticalOrdinateDimension
Represents a vertical ordinate dimension
To create or edit an instance of this class, use OrdinateDimensionBuilder Created in NX4.0.0 |
Modifier and Type | Method and Description |
---|---|
OrdinateDimension[] |
SelectOrdinateDimensionList.getArray()
Returns the list of objects in the selection list.
|
OrdinateDimension[] |
OrdinateOriginDimension.getOrdinateDimensions()
Returns ordinate dimensions of an ordinate set
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
boolean |
SelectOrdinateDimensionList.add(OrdinateDimension object)
Adds an object to the list
License requirements: None. |
boolean |
SelectOrdinateDimensionList.add(OrdinateDimension[] objects)
Adds a set of objects to the list
License requirements: None. |
boolean |
SelectOrdinateDimensionList.add(OrdinateDimension selection,
View view,
Point3d point)
Adds the object with the objects view and objects point
License requirements: None. |
boolean |
SelectOrdinateDimensionList.contains(OrdinateDimension object)
Returns whether the specified object is already in the list or not.
|
OrdinateDimensionBuilder |
DimensionCollection.createOrdinateDimensionBuilder(OrdinateDimension ordinateDimension)
|
PmiOrdinateDimensionBuilder |
DimensionCollection.createPmiOrdinateDimensionBuilder(OrdinateDimension ordinateDimension)
Creates a
PmiOrdinateDimensionBuilder
License requirements: geometric_tol ("GDT") Created in NX9.0.0 |
boolean |
SelectOrdinateDimensionList.remove(InferSnapType.SnapType snapType,
OrdinateDimension selection1,
View view1,
Point3d point1,
OrdinateDimension selection2,
View view2,
Point3d point2)
Remove specified object from list.
|
boolean |
SelectOrdinateDimensionList.remove(OrdinateDimension object)
Remove specified object from list.
|
boolean |
SelectOrdinateDimensionList.remove(OrdinateDimension object,
View view)
Remove specified object from list.
|
boolean |
SelectOrdinateDimensionList.removeArray(OrdinateDimension[] objects)
Remove specified objects from list.
|
void |
SelectOrdinateDimensionList.setArray(OrdinateDimension[] objects)
Sets the list of objects in the selection list.
|
boolean |
SelectOrdinateDimensionList.setValueWithCaeSetObjectInfo(OrdinateDimension selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObjectList.add(nxopen.TaggedObject) .
|
boolean |
SelectOrdinateDimensionList.setValueWithSnap(InferSnapType.SnapType snapType,
OrdinateDimension selection1,
View view1,
Point3d point1,
OrdinateDimension selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.