Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.HORIZONTAL_DISTANCE_BY_POSITION
horizontal distance by position, applicable only for creation
|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.HORIZONTAL_DISTANCE_FROM_ARC
horizontal distance from arc
|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.HORIZONTAL_DISTANCE_FROM_CENTER
horizontal distance from center
|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.VERTICAL_DISTANCE_BY_POSITION
vertical distance by position, applicable only for creation
|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.VERTICAL_DISTANCE_FROM_ARC
vertical distance from arc
|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.VERTICAL_DISTANCE_FROM_CENTER
vertical distance from center
|
Modifier and Type | Method and Description |
---|---|
OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.offsetMethod()
Returns the offset method
License requirements: None. |
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OffsetCenterPointBuilder.Offset |
OffsetCenterPointBuilder.Offset.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OffsetCenterPointBuilder.Offset[] |
OffsetCenterPointBuilder.Offset.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OffsetCenterPointBuilder.setOffsetMethod(OffsetCenterPointBuilder.Offset offsetMethod)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.