Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.CHIPPING |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.GRINDING |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.HAMMERING |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.MACHINING |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.NONE |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.PEENING |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.ROLLING |
Modifier and Type | Method and Description |
---|---|
LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.finishSymbol()
Returns the finishing method for the weld symbol
License requirements: None. |
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LineWeldDataBuilder.FinishSymbolType |
LineWeldDataBuilder.FinishSymbolType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LineWeldDataBuilder.FinishSymbolType[] |
LineWeldDataBuilder.FinishSymbolType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LineWeldDataBuilder.setFinishSymbol(LineWeldDataBuilder.FinishSymbolType finishSymbol)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.