Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
LineWeldDataBuilder.ContourSymbolType |
LineWeldDataBuilder.contourSymbol()
Returns the supplementary contour weld symbols that identify the shape of the weld surface or execution of a weld for both top and bottom of the reference line
License requirements: None. |
static LineWeldDataBuilder.ContourSymbolType |
LineWeldDataBuilder.ContourSymbolType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LineWeldDataBuilder.ContourSymbolType |
LineWeldDataBuilder.ContourSymbolType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LineWeldDataBuilder.ContourSymbolType[] |
LineWeldDataBuilder.ContourSymbolType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LineWeldDataBuilder.setContourSymbol(LineWeldDataBuilder.ContourSymbolType contourSymbol)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.