Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static LineWeldBuilder.FieldWeldType |
LineWeldBuilder.FieldWeldType.PLAIN |
static LineWeldBuilder.FieldWeldType |
LineWeldBuilder.FieldWeldType.TOP_FIELD |
static LineWeldBuilder.FieldWeldType |
LineWeldBuilder.FieldWeldType.TOP_FIELD_SIMPLE_FLAG |
Modifier and Type | Method and Description |
---|---|
LineWeldBuilder.FieldWeldType |
LineWeldBuilder.fieldWeld()
Returns the field indicating the weld is done at the field site
License requirements: None. |
static LineWeldBuilder.FieldWeldType |
LineWeldBuilder.FieldWeldType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LineWeldBuilder.FieldWeldType |
LineWeldBuilder.FieldWeldType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LineWeldBuilder.FieldWeldType[] |
LineWeldBuilder.FieldWeldType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LineWeldBuilder.setFieldWeld(LineWeldBuilder.FieldWeldType fieldWeld)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.