Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
LeaderData |
AnnotationManager.createLeaderData()
Creates a
LeaderData
License requirements: None. |
LeaderData |
LeaderDataList.findItem(int index)
Returns the object at the input index.
|
LeaderData[] |
LeaderDataList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LeaderDataList.append(LeaderData object)
Appends an object to the list
License requirements: None. |
void |
LeaderDataList.append(LeaderData[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
LeaderDataList.erase(LeaderData obj)
Erases the object from the list, but does not delete the object.
|
void |
LeaderDataList.erase(LeaderData obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
LeaderDataList.findIndex(LeaderData obj)
Finds the index where the input object appears.
|
void |
LeaderDataList.insert(int location,
LeaderData object)
Inserts an object at the specified location
License requirements: None. |
void |
LeaderDataList.setContents(LeaderData[] objects)
Sets the contents of the entire list.
|
void |
LeaderDataList.swap(LeaderData object1,
LeaderData object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.