Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BaseHorizontalDimension
Represents a horizontal dimension
Abstract class . |
interface |
BaseParallelDimension
Represents a parallel dimension
Abstract class . |
interface |
BaseVerticalDimension
Represents a horizontal dimension
Abstract class . |
interface |
GeneralHorizontalDimension
Represents a horizontal dimension
To obtain an instance of this class use DimensionCollection Created in NX6.0.0 |
interface |
GeneralParallelDimension
Represents a parallel dimension
To obtain an instance of this class use DimensionCollection Created in NX6.0.0 |
interface |
GeneralVerticalDimension
Represents a horizontal dimension
To obtain an instance of this class use DimensionCollection Created in NX6.0.0 |
interface |
HorizontalDimension
Represents a horizontal dimension
To create or edit an instance of this class, use LinearDimensionBuilder Created in NX4.0.0 |
interface |
ParallelDimension
Represents a parallel dimension
To create or edit an instance of this class, use LinearDimensionBuilder Created in NX4.0.0 |
interface |
PmiHorizontalDimension
Represents a PMI horizontal dimension
To create or edit an instance of this class, use PmiLinearDimensionBuilder Created in NX4.0.0 |
interface |
PmiParallelDimension
Represents a PMI parallel dimension
To create or edit an instance of this class, use PmiLinearDimensionBuilder Created in NX4.0.0 |
interface |
PmiVerticalDimension
Represents a PMI vertical dimension
To create or edit an instance of this class, use PmiLinearDimensionBuilder Created in NX4.0.0 |
interface |
VerticalDimension
Represents a vertical dimension
To create or edit an instance of this class, use LinearDimensionBuilder Created in NX4.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.