Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ArbitraryTarget
Represents an arbitrary datum target.
|
interface |
AreaTarget
Represents an area target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
BaseDatum
Represents a datum
This is an abstract class, and cannot be created. |
interface |
BaseDatumTarget
Represents a datum target
This is an abstract class, and cannot be created. |
interface |
BaseFcf
Represents a datum
This is an abstract class, and cannot be created. |
interface |
CircularTarget
Represents a circular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
Datum
Represents a datum
To create or edit an instance of this class, use PmiDatumFeatureSymbolBuilder Created in NX4.0.0 |
interface |
DatumTarget
Represents a datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingArbitraryTarget
Represents a drafting arbitrary datum target.
|
interface |
DraftingDatum
Represents a datum
To create or edit an instance of this class, use DraftingDatumFeatureSymbolBuilder Created in NX5.0.0 |
interface |
DraftingDatumTarget
Represents a datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX5.0.0 |
interface |
DraftingFcf
Represents an FCF
To create or edit an instance of this class, use DraftingFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
DraftingLineTarget
Represents a drafting line datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingPointTarget
Represents drafting point datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
Fcf
Represents an FCF
To create or edit an instance of this class, use PmiFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
LineTarget
Represents a line datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
PointTarget
Represents point datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
RectangularTarget
Represents a rectangular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
Modifier and Type | Method and Description |
---|---|
Gdt |
AnnotationManager.convertToGdt(SimpleDraftingAid draftingAid,
boolean keepDraftingAid,
LeaderBundle leader)
Converts a simple drafting aid into a GDT by creating a new GDT
using the text, origin, and preferences from the drafting aid.
|
Gdt |
AnnotationManager.createGdt(String[] textLines,
Point3d origin,
LetteringPreferences letteringPreferences,
UserSymbolPreferences userSymbolPreferences,
LineAndArrowPreferences lineArrowPreferences,
boolean alwaysVertical,
LeaderBundle leader)
Creates a GDT symbol
License requirements: drafting ("DRAFTING") . |
Modifier and Type | Method and Description |
---|---|
DraftingFeatureControlFrameBuilder |
AnnotationManager.createDraftingFeatureControlFrameBuilder(Gdt fcf)
Creates a
DraftingFeatureControlFrameBuilder
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.