Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static FractionDenominatorFormat |
FractionDenominatorFormat.EIGHT |
static FractionDenominatorFormat |
FractionDenominatorFormat.FOUR |
static FractionDenominatorFormat |
FractionDenominatorFormat.LAST
Last enum value.
|
static FractionDenominatorFormat |
FractionDenominatorFormat.ONE |
static FractionDenominatorFormat |
FractionDenominatorFormat.SIXTEEN |
static FractionDenominatorFormat |
FractionDenominatorFormat.SIXTY_FOUR |
static FractionDenominatorFormat |
FractionDenominatorFormat.THIRTY_TWO |
static FractionDenominatorFormat |
FractionDenominatorFormat.TWO |
Modifier and Type | Method and Description |
---|---|
FractionDenominatorFormat |
DimensionStyleBuilder.dualDimensionFractionDenominator()
Returns the dual dimension fractional denominator
License requirements: None. |
FractionDenominatorFormat |
DimensionPreferences.dualDimensionFractionDenominator()
Returns the dual dimension and tolerance fraction denominator
License requirements: None. |
FractionDenominatorFormat |
DimensionStyleBuilder.primaryDimensionFractionDenominator()
Returns the primary dimension fractional denominator
License requirements: None. |
FractionDenominatorFormat |
DimensionPreferences.primaryDimensionFractionDenominator()
Returns the primary dimension and tolerance fraction denominator
License requirements: None. |
static FractionDenominatorFormat |
FractionDenominatorFormat.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FractionDenominatorFormat |
FractionDenominatorFormat.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FractionDenominatorFormat[] |
FractionDenominatorFormat.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DimensionStyleBuilder.setDualDimensionFractionDenominator(FractionDenominatorFormat dualDimensionFractionDenominator)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
DimensionPreferences.setDualDimensionFractionDenominator(FractionDenominatorFormat fractionDenominator)
Sets the dual dimension and tolerance fraction denominator
License requirements: None. |
void |
DimensionStyleBuilder.setPrimaryDimensionFractionDenominator(FractionDenominatorFormat primaryDimensionFractionDenominator)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
DimensionPreferences.setPrimaryDimensionFractionDenominator(FractionDenominatorFormat fractionDenominator)
Sets the primary dimension and tolerance fraction denominator
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.