Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
FeatureControlFrameIndicatorBuilder |
AnnotationManager.createFeatureControlFrameIndicatorBuilder()
Creates a
FeatureControlFrameIndicatorBuilder
License requirements: None. |
FeatureControlFrameIndicatorBuilder |
FeatureControlFrameIndicatorBuilderList.findItem(int index)
Returns the object at the input index.
|
FeatureControlFrameIndicatorBuilder[] |
FeatureControlFrameIndicatorBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FeatureControlFrameIndicatorBuilderList.append(FeatureControlFrameIndicatorBuilder object)
Appends an object to the list
License requirements: None. |
void |
FeatureControlFrameIndicatorBuilderList.append(FeatureControlFrameIndicatorBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FeatureControlFrameIndicatorBuilderList.erase(FeatureControlFrameIndicatorBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
FeatureControlFrameIndicatorBuilderList.erase(FeatureControlFrameIndicatorBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FeatureControlFrameIndicatorBuilderList.findIndex(FeatureControlFrameIndicatorBuilder obj)
Finds the index where the input object appears.
|
void |
FeatureControlFrameIndicatorBuilderList.insert(int location,
FeatureControlFrameIndicatorBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
FeatureControlFrameIndicatorBuilderList.setContents(FeatureControlFrameIndicatorBuilder[] objects)
Sets the contents of the entire list.
|
void |
FeatureControlFrameIndicatorBuilderList.swap(FeatureControlFrameIndicatorBuilder object1,
FeatureControlFrameIndicatorBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.