Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection |
FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection.AFTER |
static FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection |
FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection.BEFORE |
Modifier and Type | Method and Description |
---|---|
FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection |
FeatureControlFrameIndicatorBuilder.direction()
Returns the direction
License requirements: None. |
static FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection |
FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection |
FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection[] |
FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FeatureControlFrameIndicatorBuilder.setDirection(FeatureControlFrameIndicatorBuilder.FcfIndicatorDirection direction)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.