Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.ANGULAR |
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.INCLUDING |
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.PARALLEL |
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.PERPENDICULAR |
Modifier and Type | Method and Description |
---|---|
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.symbol()
Returns the charactersitic
License requirements: None. |
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic[] |
FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FeatureControlFrameIndicatorBuilder.setSymbol(FeatureControlFrameIndicatorBuilder.FcfIndicatorCharacteristic symbol)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.