Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
FeatureControlFrameDataBuilder |
AnnotationManager.createFeatureControlFrameDataBuilder(FeatureControlFrameData frame)
Creates a
FeatureControlFrameDataBuilder
License requirements: None. |
FeatureControlFrameDataBuilder[] |
FeatureControlFrameBuilder.featureControlFrameData()
The feature control frame data list. this method will always return at least two frames. for single feature control frames
(frame type is single frame type) only the first frame is used.
|
FeatureControlFrameDataBuilder |
FeatureControlFrameDataBuilderList.findItem(int index)
Returns the object at the input index.
|
FeatureControlFrameDataBuilder[] |
FeatureControlFrameDataBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FeatureControlFrameDataBuilderList.append(FeatureControlFrameDataBuilder object)
Appends an object to the list
License requirements: None. |
void |
FeatureControlFrameDataBuilderList.append(FeatureControlFrameDataBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FeatureControlFrameDataBuilderList.erase(FeatureControlFrameDataBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
FeatureControlFrameDataBuilderList.erase(FeatureControlFrameDataBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FeatureControlFrameDataBuilderList.findIndex(FeatureControlFrameDataBuilder obj)
Finds the index where the input object appears.
|
void |
FeatureControlFrameDataBuilderList.insert(int location,
FeatureControlFrameDataBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
FeatureControlFrameDataBuilderList.setContents(FeatureControlFrameDataBuilder[] objects)
Sets the contents of the entire list.
|
void |
FeatureControlFrameDataBuilderList.swap(FeatureControlFrameDataBuilder object1,
FeatureControlFrameDataBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.