Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static ExtensionLineDisplay |
ExtensionLineDisplay.FIRST
Displays extension line attached to the
first object selected to create the dimension
|
static ExtensionLineDisplay |
ExtensionLineDisplay.LAST
Last enum value.
|
static ExtensionLineDisplay |
ExtensionLineDisplay.NONE
Doesn't display extension lines
|
static ExtensionLineDisplay |
ExtensionLineDisplay.SECOND
Displays extension line attached to the
second object selected to create the dimension
|
static ExtensionLineDisplay |
ExtensionLineDisplay.TWO
Displays both the extension lines
|
Modifier and Type | Method and Description |
---|---|
ExtensionLineDisplay |
DimensionStyleBuilder.extensionLineDisplay()
Returns the extension line display option.
|
ExtensionLineDisplay |
DimensionPreferences.extensionLineDisplay()
Returns the extension line display
License requirements: None. |
static ExtensionLineDisplay |
ExtensionLineDisplay.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtensionLineDisplay |
ExtensionLineDisplay.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtensionLineDisplay[] |
ExtensionLineDisplay.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DimensionStyleBuilder.setExtensionLineDisplay(ExtensionLineDisplay extensionLineDisplay)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
DimensionPreferences.setExtensionLineDisplay(ExtensionLineDisplay display)
Sets the extension line display
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.