Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static DrivingValueBuilder.DrivingExpressionMode |
DrivingValueBuilder.DrivingExpressionMode.KEEP_EXPRESSION |
static DrivingValueBuilder.DrivingExpressionMode |
DrivingValueBuilder.DrivingExpressionMode.MEASURE_GEOMETRY |
Modifier and Type | Method and Description |
---|---|
DrivingValueBuilder.DrivingExpressionMode |
DrivingValueBuilder.expressionMode()
Returns the expression mode
License requirements: None. |
static DrivingValueBuilder.DrivingExpressionMode |
DrivingValueBuilder.DrivingExpressionMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrivingValueBuilder.DrivingExpressionMode |
DrivingValueBuilder.DrivingExpressionMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrivingValueBuilder.DrivingExpressionMode[] |
DrivingValueBuilder.DrivingExpressionMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrivingValueBuilder.setExpressionMode(DrivingValueBuilder.DrivingExpressionMode expressionMode)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.