Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.ANGULAR
Angular measurement type
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.CYLINDRICAL
Linear measurement method representing a diameter
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.DIAMETRAL
Diametral measurement type
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.HOLE_CALLOUT
Hole Callout based measurement
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.HORIZONTAL
Horizontal measurement direction
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.INFERRED
Inferred measurement direction (UI Only)
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.PERPENDICULAR
Perpendicular measurement direction
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.POINT_TO_POINT
Point to point measurement direction
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.RADIAL
Radial measurement type
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.VERTICAL
Vertical measurement direction
|
Modifier and Type | Method and Description |
---|---|
DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.method()
Returns the measurement method for the size of the dimension
License requirements: None. |
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DimensionMeasurementBuilder.MeasurementMethod |
DimensionMeasurementBuilder.MeasurementMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DimensionMeasurementBuilder.MeasurementMethod[] |
DimensionMeasurementBuilder.MeasurementMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DimensionMeasurementBuilder.setMethod(DimensionMeasurementBuilder.MeasurementMethod method)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") OR solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.