Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static CircleCenterlineBuilder.Types |
CircleCenterlineBuilder.Types.CENTERPOINT
Centerline using Centerpoint Method
|
static CircleCenterlineBuilder.Types |
CircleCenterlineBuilder.Types.THROUGH3POINTS
Centerline using 3 or More Points Method
|
Modifier and Type | Method and Description |
---|---|
CircleCenterlineBuilder.Types |
CircleCenterlineBuilder.type()
Returns the method which returns type of centerline
License requirements: None. |
static CircleCenterlineBuilder.Types |
CircleCenterlineBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CircleCenterlineBuilder.Types |
CircleCenterlineBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CircleCenterlineBuilder.Types[] |
CircleCenterlineBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CircleCenterlineBuilder.setType(CircleCenterlineBuilder.Types method)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.