Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BaseBoltCircleCenterline
Represents a base bolt centerline class
This is an abstract class. |
interface |
BoltCircleCenterline
Represents a BoltCircleCenterline centerline
To create or edit an instance of this class, use BoltCircleCenterlineBuilder Created in NX6.0.0 |
interface |
CircularCenterline
Represents a CircularCenterline centerline
To create or edit an instance of this class, use CircularCenterlineBuilder Created in NX6.0.0 |
interface |
PmiBoltCircleCenterline
Represents a PMI Bolt Circle Centerline class
To create or edit an instance of this class, use PmiBoltCircleCenterlineBuilder Created in NX12.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.