Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static ChamferOrientationType |
ChamferOrientationType.HORIZONTAL
default (same as the adjacent edge)
|
static ChamferOrientationType |
ChamferOrientationType.PARALLEL
parallel to the chamfer line itself
|
static ChamferOrientationType |
ChamferOrientationType.VERTICAL
perpendicular with default
|
Modifier and Type | Method and Description |
---|---|
ChamferOrientationType |
BaseChamferDimension.chamferOrientation()
Returns a value of chamfer dimension linear leader parallel
License requirements: None. |
ChamferOrientationType |
BaseChamferDimensionBuilder.orientation()
Returns the orientation of linear chamfer dimension
License requirements: None. |
static ChamferOrientationType |
ChamferOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ChamferOrientationType |
ChamferOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ChamferOrientationType[] |
ChamferOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseChamferDimension.setChamferOrientation(ChamferOrientationType orientation)
Sets a value of chamfer dimension linear leader parallel
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
BaseChamferDimensionBuilder.setOrientation(ChamferOrientationType orientation)
License requirements: drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.