Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.BILATERAL
Bilateral
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.EQUAL_BILATERAL
Equal bilateral
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.MINUS_LIMIT_ONE_LINE
Minus limit one line
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.MINUS_LIMIT_TWO_LINES
Minus limit two lines
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.NONE
No tolerance
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.PLUS_LIMIT_ONE_LINE
Plus limit one line
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.PLUS_LIMIT_TWO_LINES
Plus limit two lines
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.UNILATERAL_MINUS
Unilateral minus
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.UNILATERAL_PLUS
Unilateral plus
|
Modifier and Type | Method and Description |
---|---|
BaseSurfaceFinishBuilder.ToleranceOption |
SurfaceFinishBuilder.toleranceType()
Returns the tolerance type is applicable only where Material Removal is required
License requirements: None. |
BaseSurfaceFinishBuilder.ToleranceOption |
DraftingSurfaceFinishBuilder.toleranceType()
Returns the tolerance type applicable only for all the 3 cases of finish type where Material Removal Required
License requirements: None. |
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseSurfaceFinishBuilder.ToleranceOption |
BaseSurfaceFinishBuilder.ToleranceOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseSurfaceFinishBuilder.ToleranceOption[] |
BaseSurfaceFinishBuilder.ToleranceOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SurfaceFinishBuilder.setToleranceType(BaseSurfaceFinishBuilder.ToleranceOption toleranceType)
License requirements: None. |
void |
DraftingSurfaceFinishBuilder.setToleranceType(BaseSurfaceFinishBuilder.ToleranceOption toleranceType)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.