Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DraftingSurfaceFinish
Represents a Drafting Surface Finish
To create or edit an instance of this class, use DraftingSurfaceFinishBuilder Created in NX7.5.0 |
interface |
SurfaceFinish
Represents a PMI Surface Finish
To create or edit an instance of this class, use SurfaceFinishBuilder Created in NX6.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
DraftingSurfaceFinishBuilder.inheritFrom(BaseSurfaceFinish inheritTag)
The drafting surface finish is inherited form existing drafting surface finish.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.