Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DraftingFcf
Represents an FCF
To create or edit an instance of this class, use DraftingFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
Fcf
Represents an FCF
To create or edit an instance of this class, use PmiFeatureControlFrameBuilder Created in NX4.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
FeatureControlFrameBuilder.inheritFrom(BaseFcf inheritTag)
The feature control frame is inherited form existing feature control frame.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.