Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ArbitraryTarget
Represents an arbitrary datum target.
|
interface |
AreaTarget
Represents an area target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
CircularTarget
Represents a circular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
DatumTarget
Represents a datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingArbitraryTarget
Represents a drafting arbitrary datum target.
|
interface |
DraftingDatumTarget
Represents a datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX5.0.0 |
interface |
DraftingLineTarget
Represents a drafting line datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingPointTarget
Represents drafting point datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
LineTarget
Represents a line datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
PointTarget
Represents point datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
RectangularTarget
Represents a rectangular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
DatumTargetBuilder.inheritFrom(BaseDatumTarget inheritTag)
The datum target is inherited form existing datum target.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.