Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static ArrowDisplay |
ArrowDisplay.FIRST
Displays arrow to the first object selected to create
the dimension
|
static ArrowDisplay |
ArrowDisplay.LAST
Last enum value.
|
static ArrowDisplay |
ArrowDisplay.NONE
Doesn't display arrows
|
static ArrowDisplay |
ArrowDisplay.SECOND
Displays arrow to the second object selected to create
the dimension
|
static ArrowDisplay |
ArrowDisplay.TWO
Displays both the arrows
|
Modifier and Type | Method and Description |
---|---|
ArrowDisplay |
DimensionPreferences.arrowDisplay()
Returns the arrow display
License requirements: None. |
ArrowDisplay |
DimensionStyleBuilder.dimArrowDisplay()
Returns the dimension arrow display option
License requirements: None. |
static ArrowDisplay |
ArrowDisplay.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ArrowDisplay |
ArrowDisplay.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ArrowDisplay[] |
ArrowDisplay.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DimensionPreferences.setArrowDisplay(ArrowDisplay display)
Sets the arrow display
License requirements: None. |
void |
DimensionStyleBuilder.setDimArrowDisplay(ArrowDisplay dimArrowDisplay)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.