Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
ArbitraryAreaSeedBuilder |
PmiManager.createArbitraryAreaSeedBuilder()
Creates a
ArbitraryAreaSeedBuilder
License requirements: None. |
ArbitraryAreaSeedBuilder |
ArbitraryAreaSeedBuilderList.findItem(int index)
Returns the object at the input index.
|
ArbitraryAreaSeedBuilder[] |
ArbitraryAreaSeedBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ArbitraryAreaSeedBuilderList.append(ArbitraryAreaSeedBuilder object)
Appends an object to the list
License requirements: None. |
void |
ArbitraryAreaSeedBuilderList.append(ArbitraryAreaSeedBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ArbitraryAreaSeedBuilderList.erase(ArbitraryAreaSeedBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ArbitraryAreaSeedBuilderList.erase(ArbitraryAreaSeedBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ArbitraryAreaSeedBuilderList.findIndex(ArbitraryAreaSeedBuilder obj)
Finds the index where the input object appears.
|
void |
ArbitraryAreaSeedBuilderList.insert(int location,
ArbitraryAreaSeedBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ArbitraryAreaSeedBuilderList.setContents(ArbitraryAreaSeedBuilder[] objects)
Sets the contents of the entire list.
|
void |
ArbitraryAreaSeedBuilderList.swap(ArbitraryAreaSeedBuilder object1,
ArbitraryAreaSeedBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.