Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Method and Description |
---|---|
SketchAngularDimensionBuilder |
SketchCollection.createAngularDimensionBuilder(AngularDimension angularDimension)
Creates a
SketchAngularDimensionBuilder
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") Created in NX9.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
GeneralMajorAngularDimension
Represents a major angular dimension
To obtain an instance of this class use DimensionCollection Created in NX6.0.0 |
interface |
GeneralMinorAngularDimension
Represents a minor angular dimension
To obtain an instance of this class use DimensionCollection Created in NX6.0.0 |
interface |
MajorAngularDimension
Represents a major angular dimension
To create or edit an instance of this class, use MajorAngularDimensionBuilder Created in NX4.0.0 |
interface |
MinorAngularDimension
Represents a minor angular dimension
To create or edit an instance of this class, use MinorAngularDimensionBuilder Created in NX4.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.