public static class SearchCriteriaDimensionBuilder.ToleranceTypes extends Enum
Modifier and Type | Method and Description |
---|---|
static SearchCriteriaDimensionBuilder.ToleranceTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SearchCriteriaDimensionBuilder.ToleranceTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SearchCriteriaDimensionBuilder.ToleranceTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final SearchCriteriaDimensionBuilder.ToleranceTypes NO_TOLERANCE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes EQUAL_BILATERAL_TOLERANCE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes BILATERAL_TOLERANCE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes UNILATERAL_PLUS
public static final SearchCriteriaDimensionBuilder.ToleranceTypes UNILATERAL_MINUS
public static final SearchCriteriaDimensionBuilder.ToleranceTypes PLUS_LIMIT_TWO_LINES
public static final SearchCriteriaDimensionBuilder.ToleranceTypes MINUS_LIMIT_TWO_LINES
public static final SearchCriteriaDimensionBuilder.ToleranceTypes PLUS_LIMIT_ONE_LINE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes MINUS_LIMIT_ONE_LINE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes LIMITS_AND_FITS
public static final SearchCriteriaDimensionBuilder.ToleranceTypes BASIC
public static final SearchCriteriaDimensionBuilder.ToleranceTypes REFERENCE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes DIAMETER_REFERENCE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes NOT_TO_SCALE
public static final SearchCriteriaDimensionBuilder.ToleranceTypes BASIC_DIMENSION_NOT_TO_SCALE
public static final int _NO_TOLERANCE
public static final int _EQUAL_BILATERAL_TOLERANCE
public static final int _BILATERAL_TOLERANCE
public static final int _UNILATERAL_PLUS
public static final int _UNILATERAL_MINUS
public static final int _PLUS_LIMIT_TWO_LINES
public static final int _MINUS_LIMIT_TWO_LINES
public static final int _PLUS_LIMIT_ONE_LINE
public static final int _MINUS_LIMIT_ONE_LINE
public static final int _LIMITS_AND_FITS
public static final int _BASIC
public static final int _REFERENCE
public static final int _DIAMETER_REFERENCE
public static final int _NOT_TO_SCALE
public static final int _BASIC_DIMENSION_NOT_TO_SCALE
public static SearchCriteriaDimensionBuilder.ToleranceTypes valueOf(int value)
public static SearchCriteriaDimensionBuilder.ToleranceTypes valueOf(String name)
public static SearchCriteriaDimensionBuilder.ToleranceTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.