public static class HumanData.InverseKinematicsBalanceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALLOW_STEP
Indicate human is allowed to move one step to keep balance
|
static int |
_KEEP_SEATED
Indicate human is in a seated position and thus supported by the lower torso
|
static int |
_NO_STEP
Indicate human foot is fixate without step
|
static HumanData.InverseKinematicsBalanceType |
ALLOW_STEP
Indicate human is allowed to move one step to keep balance
|
static HumanData.InverseKinematicsBalanceType |
KEEP_SEATED
Indicate human is in a seated position and thus supported by the lower torso
|
static HumanData.InverseKinematicsBalanceType |
NO_STEP
Indicate human foot is fixate without step
|
Modifier and Type | Method and Description |
---|---|
static HumanData.InverseKinematicsBalanceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.InverseKinematicsBalanceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.InverseKinematicsBalanceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final HumanData.InverseKinematicsBalanceType ALLOW_STEP
public static final HumanData.InverseKinematicsBalanceType NO_STEP
public static final HumanData.InverseKinematicsBalanceType KEEP_SEATED
public static final int _ALLOW_STEP
public static final int _NO_STEP
public static final int _KEEP_SEATED
public static HumanData.InverseKinematicsBalanceType valueOf(int value)
public static HumanData.InverseKinematicsBalanceType valueOf(String name)
public static HumanData.InverseKinematicsBalanceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.