public interface BodyCollection extends TaggedObjectCollection
Part
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
void |
collectionSweepabilityCheck(boolean setColor)
Sweepability check
License requirements: solid_modeling ("SOLIDS MODELING") . |
FlatteningBuilder |
createFlatteningBuilder()
Deprecated.
Deprecated in NX11.0.0. Use
FlatteningAndFormingBuilder instead.
|
FourPointSurfaceBuilder |
createFourPointSurfaceBuilder()
Creates a Four Point Surface Builder
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
SurfaceUVDirectionBuilder |
createSurfaceUvdirectionBuilder()
Creates a SurfaceUVDirectionBuilder
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Body |
findObject(String journalIdentifier)
Finds the
Body with the given identifier as recorded in a journal. |
_find_next, iterator
Body findObject(String journalIdentifier) throws NXException, RemoteException
Body
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Identifier of the body you wantNXException
RemoteException
FourPointSurfaceBuilder createFourPointSurfaceBuilder() throws NXException, RemoteException
NXException
RemoteException
SurfaceUVDirectionBuilder createSurfaceUvdirectionBuilder() throws NXException, RemoteException
NXException
RemoteException
FlatteningBuilder createFlatteningBuilder() throws NXException, RemoteException
FlatteningAndFormingBuilder
instead.
FlatteningBuilder
.
NXException
RemoteException
void collectionSweepabilityCheck(boolean setColor) throws NXException, RemoteException
setColor
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.